EIO0000005603.01

Precautions for Building into an End-use Product

This product is designed for use on flat surfaces of IP66, UL 50/50E or Type 4X (indoor use only) enclosure.

Be aware of the following when building this product into an end-use product:

  • The rear face of this product is not approved as an enclosure. When building this product into an end-use product, be sure to use an enclosure that satisfies standards as the end-use product's overall enclosure.

  • Install this product in an enclosure with mechanical rigidity.

  • This product is an open type device and not designed for outdoor use. UL certification obtained is for indoor use only.

  • Install and operate this product with its front panel facing outward.

NOTE: IP66 is not part of UL certification.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.