NVE3860502-10

Button functions in editing Clear parameters

The meter supports single press functions of the buttons to enter Clear screens.
Mode Button Function
Clear Screen

Press and hold OK button for 2 seconds to enter Clear.

Press OK button to clear/reset parameter values.

Press and hold OK button for 2 seconds to exit Clear.

To navigate to the next parameter.
To navigate to the previous parameter.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.