NVE3860502-10

Demand

The meter provides last, present, predicted, and maximum (peak) demand values, and a timestamp when the maximum (peak) demand occurred.

The meter supports standard demand calculation methods, including sliding block, fixed block, rolling block, thermal and synchronized.

Peak demand registers can be reset manually (password protected).

Demand measurements include:

  • W, VAR, VA demand total

  • Amps demand average

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.