NVE3860502-10

Peak demand

The meter records the peak (or maximum) values for kWD, kVARD, and kVAD power (or peak demand).

The peak for each value is the highest average reading since the meter was last reset. These values are maintained in the meter’s non-volatile memory.

The meter also stores the date and time when the peak demand occurred.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.