NVE3860502-10

Lock / Unlock

Lock enables you to set the a meter screen to default screen. You can scroll to other display screens while a screen has been locked. Once the manual scrolling is stopped, the meter displays the default (lock) screen after four minutes.

The meter’s display screen and buttons allow you to lock or unlock any screen.

To lock / unlock a meter screen:

  • Press and hold the Up and OK buttons simultaneously for 2 seconds to lock or unlock a meter screen.

NOTE:

You can only lock the display parameters.

You cannot enter the Setup or Clear when a meter screen is locked.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.