NVE3860502-10

PM2125C meter model

The PM2125C meter is available in one physical form factor and variant.

Meter models

Model Commercial reference Description
PM2125C METSEPM2125C Class 1 panel mount LED meter with RS-485 communication and digital I/O capabilities.
METSEPM2125CL05 Class 0.5S panel mount LED meter with RS-485 communication and digital I/O capabilities.
METSEPM2125C2AI2AO Class 0.5S panel mount LED meter with RS-485 communication and analog I/O capabilities.
METSEPM2125C2DI2RO Class 0.5S panel mount LED meter with RS-485 communication and relay output capabilities.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?