NVE3860502-10

Other measurements

Additional measurements recorded by the meter include several timers.

These timers include:

  • I/O timer displays the powered ON duration of the input or output.

  • Operating timer displays the powered ON duration of the meter.

  • Active load timer displays the duration of the connected load, based on the specified minimum current for the load timer setpoint setting.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.