NVE3860502-10

Feature summary

Parameter

PM2125C

Accuracy Class for Wh

Class 1 or Class 0.5S

Accuracy Class for VARh

Class 1

Sampling rate per cycle

64

Current:

  • Per-phase and 3 phase average

  • Calculated neutral current

ü

Voltage:

  • V L-N - per-phase and 3 phase average

  • V L-L - per-phase and 3 phase average

ü

Power factor

  • Per phase and 3 phase total

True PF

Displacement PF *

Frequency

ü

Power:

  • Active power (kW) - Phase wise and total

  • Apparent power (kVA) - Phase wise and total

  • Reactive power (kVAR) - Phase wise and total

ü

3 Phase unbalance

Current

Voltage *

Demand parameters (kW, kVA, kVAR, I)

  • Last demand

  • Present demand

  • Predictive demand

  • Peak demand: Timestamp for peak demand *

ü

Energy: kWh, kVAh, kVARh (4 Quadrant)

  • Delivered (Import / Forward)

  • Received (Export / Reverse)

Delivered (D)

Received (R)

Total (D+R) *

Net (D-R) *

Last cleared (Old) *

Meter On hours

Load Run hours

Power Interruptions

ü

THD %:

  • Voltage L-N per phase

  • Voltage L-L per phase

  • Current per phase

ü

Individual Harmonics *

Up to 15th individual harmonics

Min / Max with timestamp *

  • V L-L average

  • V L-N average

  • Current average

  • Frequency

  • Active power, Total

  • Apparent power, Total

  • Reactive power, Total

  • Power factor, Total

ü

RTC with battery backup

ü

Communication

RS-485 Modbus RTU

Digital IO modules (2 inputs & 2 outputs)

Applicable for METSEPM2125C and METSEPM2125CL05

Analog IO modules (2 inputs & 2 outputs)

Applicable for METSEPM2125C2AI2AO

Relay IO modules (2 digital inputs and 2 relay outputs)

Applicable for METSEPM2125C2DI2RO

Retrofit (RtFt)

For configuring legacy communication data models

ü
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.