NVE3860502-10

Meter battery

The internal battery in the meter keeps the meter’s clock running when it is powered down to help maintain the meter time.

The life expectancy of the meter’s internal battery is estimated to be over 10 years at 25 °C under typical operating conditions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.