NVE3860502-10

Button functions in editing setup parameters

The meter supports single press and combination press functions of the buttons to edit setup parameters.
Mode Button Function
Setup Menu

Flashing Digit: To decrease the numeric value.

Flashing Value: To view the next value from the list.

Flashing Decimal Point: To move the decimal point to the left.

Flashing Digit: To increase the numeric value.

Flashing Value: To view the previous value from the list.

Flashing Decimal Point: To move the decimal point to the right.

Press and hold for 2 seconds.

Flashing Digit / Flashing Decimal Point: To move the position of the cursor to left.

Press and hold for 2 seconds.

Flashing Digit / Flashing Decimal Point: To move the position of the cursor to right.

To select a parameter to edit the values.

To select configured parameter values.

To save the changes made to setup parameter.

  

Press and hold the Up and Down buttons simultaneously for 2 seconds to enter Setup.

Exit setup with the same button sequence.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.