NVE3860502-10

Using software to view meter data

There are different software systems and methods you can use to access or display the meter data. This can range from using a simple Modbus register interface to read stored values in the meter’s registers, to viewing intelligent information from the meter through an energy management system.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.