NVE3860502-10

Exiting setup parameters

The following steps describe how to exit setup mode without editing any parameter values.
  1. Press and hold the Up and Down buttons simultaneously for 2 seconds to enter Setup.
  2. Enter password. Default password is 0000.
  3. Press OK.
  4. Press the Up or Down button to view various setup parameters.
  5. Press and hold the Up and Down buttons simultaneously for 2 seconds to exit Setup without making any changes to the parameter values.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.