NVE3860502-10

Entering Clear screen

The meter’s display screen and buttons allow you to navigate to Clear.
  1. Press and hold the OK button for 2 seconds.
  2. Press the Up button to select Yes.
  3. Press OK.
  4. Enter password. Default password is 0000.
  5. Press OK.
  6. Press the Down or Up button to navigate to the required parameter for clearing the values.
  7. Press and hold the OK button simultaneously for 2 seconds to exit Clear screen.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.