NVE3860502-10

About this manual

This manual discusses features of the EasyLogic™ PM2125 power meter and provides installation and configuration instructions.

Throughout the manual, the term “meter” refers to all models of the PM2125. All differences between the models, such as a feature specific to one model, are indicated with the appropriate model number or description.

This manual assumes you have an understanding of power metering and are familiar with the equipment and power system in which your meter is installed.

This manual does not provide configuration information for advanced features where an expert user would perform advanced configuration. It also does not include instructions on how to incorporate meter data or perform meter configuration using energy management systems or software, other than ION Setup. ION Setup is a free configuration tool available for download from www.se.com.

The most up-to-date documentation about your meter is available for download from www.se.com.

Related documents

Document Number

PM2125 instruction sheet

NHA2779001

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.