NVE3860502-10

Viewing firmware version, model and serial number

You can view the meter’s firmware version, model and serial number from the display panel.
  1. Press and hold Down and OK button for 2 seconds to enter Diag page. Meter display shows all LEDs turned on.
  2. Press Down button to view meter model, serial number, OS version, and RS version.
  3. Press and hold Down and OK button for 2 seconds to exit Diag page.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.