NVE3860502-10

Display overview

The display lets you use the meter to perform various tasks such as setting up the meter, displaying data screens, or performing resets.

A

Phase measurements

VL-N, VL-L, I, kVA, kW, kVAR, PF, VTHD, ITHD

B

Demand measurements

DM, PrsDM, PrdDM, MD

C

RTC (Amber) / IO (Green)

D

Negative indicator

E

Navigation key

To navigate down

F

Energy readings

Apparent energy, Active energy, and Reactive energy

G

Navigation key

To navigate up

H

OK

Enter key

I

Energy pulsing LED (Red)

Heartbeat / communications LED (Green)

J

x 1000 indicator

K

System measurements

Vavg, kVA, F, Iavg, kW, In, PFavg, kVAR, Iunb

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.