NVE3860502-10

Button functions in locking / unlocking meter screen

The meter supports a combination press function of the buttons to lock or unlock a screen.
Mode Button Function
Lock / Unlock   

Press and hold the Up and OK buttons simultaneously for 2 seconds to lock or unlock a meter screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.