NVE3860502-10

Setting up date and time

The Clock setup allows you to set the meter’s date and time.
  1. Press and hold the Up and Down buttons simultaneously for 2 seconds to enter Setup.

  2. Enter password. Default password is 0000.

  3. Press OK.

  4. Press the Down button to select year, date, and hour parameter.

  5. Press OK.

  6. Press Down button to change the digits.

    NOTE: Hold the Down button for 2 seconds to move the cursor to the next digit.
  7. Press OK.

  8. Press and hold the Up and Down buttons simultaneously for 2 seconds to exit Setup.

  9. Select Yes to save your settings.

NOTE: You must always set or sync the meter time to local time.

Clock setup parameters

Parameter Values Description
Year YYYY Set the current year using format displayed on screen.
Date MM:DD Set the current date using the format displayed on screen, where date is in MM (month) and DD (date) format.
Hour HH:MM Use the 24 hours format to set the current time in local time, where the time is in HH (hour) and MM (minutes) format.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.