NVE3860502-10

Meter initialization

Meter Initialization is a special command that clears the meter’s energy, power, demand values, and meter operation timer.

It is common practice to initialize the meter after its configuration is completed, before adding it to an energy management system.

After configuring all the meter setup parameters, navigate through the different meter display screens and make sure the displayed data is valid then perform meter initialization.

NOTE: You can perform meter initialization using ION setup and secured command interface.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.