NVE3860502-10

Demand parameters

Demand is a measure of average consumption (typically power or current) over a fixed programmed time interval.

Power / current demand setup parameters

Parameter Values Description
Method
  • Thermal: Ther

  • Timed Sliding Block: t.Sb

  • Timed Block: t.b

  • Timed Rolling Block: t.rb

  • Command Sync Block: CS.b

  • Command Sync Rolling Block: CS.rb

  • Clock Sync Block: CL.b

  • Clock Sync Rolling Block: Cl.rb

NOTE: Command sync and clock sync methods are applicable for meters with RS-485 communication only.

Select the appropriate demand calculation method for your needs.

Interval 1 – 60

Set the demand interval, in minutes.

Subinterval (update time) 1 – 60

Applies only to rolling block methods.

Define how many subintervals the demand interval should be equally divided into.

Clock Sync Time 00:00 – 23:59

Applies only to clock sync methods (these synchronize the demand interval to the meter’s internal clock).

Define what time of day you want to synchronize the demand.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.