DOCA0128EN-02

FLCmin

Minimum Full Load Current. The smallest amount of motor current the LTMR controller will support. This value is determined by the LTMR controller model.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?