IEC Format Wiring Diagrams
Overview
This section contains the wiring diagrams corresponding to the five pre-configured operating modes:
|
Overload |
Monitoring of the motor load where control (start/stop) of the motor load is achieved by a mechanism other than the controller |
|
Independent |
Direct-on-line (across-the-line) full-voltage non-reversing motor starting applications |
|
Reverser |
Direct-on-line (across-the-line) full-voltage reversing motor starting applications |
|
Two-Step |
Reduced voltage starting motor applications, including:
|
|
Two-Speed |
Two-speed motor applications for motor types, including:
|
Each application is described individually, with:
|
One complete application diagram (including power and control) |
3-wire (impulse) terminal strip control |
|
Three partial diagrams (control logic input wiring variants) |
2-wire (maintained) terminal strip control |
|
3-wire (impulse) terminal strip control with network control selectable |
|
|
2-wire (maintained) terminal strip control with network control selectable |