Communication Alarms and Trips
Introduction
Communication alarms and trips are managed in a standard way, like any other types of alarms and trips.
The presence of a trip is signaled by various indicators:
-
State of the LEDs:
-
On LTMR Ethernet controllers: 3 LEDs are dedicated to communication, 1 STS LED and 2 LK/ACT LEDs, one for each network port connector.
-
On LTMR Modbus controllers: 1 LED is dedicated to communication, PLC Comm.
-
On LTMR PROFIBUS DP controllers: 1 LED is dedicated to communication, BF.
-
On LTMR CANopen controllers: 1 LED is dedicated to communication, Status.
-
On LTMR DeviceNet controllers: 1 LED is dedicated to communication, MNS.
-
-
State of the output relays
-
Alarm
-
Message(s) displayed on HMI screen
-
Presence of an exception code (such as a report from the PLC)
PLC Communication Loss
A communication loss is managed like any other trip.
The LTMR controller monitors the communication with the PLC. Using an adjustable network idle time (timeout), the LTMR controller watchdog function can report a network loss (firmware watchdog).
In the event of a network loss, the LTMR controller can be configured to take certain actions. These depend on the control mode that the LTMR controller was operating in prior to the network loss.
If PLC-LTMR controller communication is lost while the LTMR controller is in network control mode, the LTMR controller enters the fallback state. If PLC- LTMR controller communication is lost while the LTMR controller is in local control mode, and then the control mode is changed to network control, the LTMR controller enters the fallback state.
If PLC-LTMR controller communication is restored while the control mode is set to network control, the LTMR controller exits the fallback state. If the control mode is changed to local control, the LTMR exits from the fallback state, regardless of the state of PLC-controller communications.
The table below defines the available actions that the LTMR controller can take during a communication loss that the user can select when configuring the LTMR controller.
Network communication loss actions:
|
LTMR Controller Output Control Mode Prior to Network Loss |
Available LTMR Actions After PLC-LTMR Controller Network Loss |
|---|---|
|
Terminal Strip and HMI control |
Trip and Alarm control possibilities:
|
|
Network control |
Trip and Alarm control possibilities:
|
HMI Communication Loss
The LTMR controller monitors the communication with any approved HMI device. Using a fixed network idle time (timeout), the LTMR controller watchdog function can report a network loss. In the event of a communication loss, the LTMR controller can be configured to take certain actions. These depend on the control mode that the LTMR controller was operating in prior to the communication loss.
If HMI-controller communication is lost while the LTMR controller is in HMI control mode, the LTMR controller enters the fallback state. If HMI-LTMR controller communication is lost while the LTMR controller is not in HMI control mode, and then the control mode is changed to HMI control, the LTMR controller enters the fallback state.
If HMI-controller communication is restored while the control mode is set to HMI control, the LTMR exits from the fallback state. If the control mode is changed to Terminal Strip or Network control, the LTMR exits from the fallback state, regardless of the state of HMI-controller communications.
The following table defines the available actions that the LTMR controller may take during a communication loss. Select one of these actions when configuring the LTMR controller.
|
LTMR Controller Output Control Mode Prior to HMI Loss |
Available LTMR Controller Actions After HMI-LTMR Controller HMI Loss |
|---|---|
|
Terminal Strip and network control |
Trip and Alarm control possibilities:
|
|
HMI control |
Trip and Alarm control possibilities:
|