DOCA0128EN-02

Wiring Diagrams

Overview

The LTMR operating mode wiring diagrams can be drawn according to IEC or NEMA standards.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Turn off all power supplying this equipment before working on it.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices.
Failure to follow these instructions will result in death or serious injury.
NOTICE
LOGIC INPUTS DESTRUCTION HAZARD
  • Connect the LTMR controller's inputs using the three Common (C) terminals connected to the A1 control voltage via an internal filter.
  • Do not connect the Common (C) terminal to the A1 or A2 control voltage inputs.
Failure to follow these instructions can result in equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.