First Power-up
Overview
First power-up describes the first time power is cycled to:
-
A new LTMR controller, or
-
An LTMR controller that has been previously commissioned, but whose parameter settings have been restored to the factory settings, either as a result of:
-
Execution of the Clear All Command, or
-
A firmware upgrade
-
On first power-up, the LTMR controller enters a locked, non-configured state, called the initialized state, and the Controller System Config Required parameter is turned On. The LTMR controller exits this state only after certain parameters, called required parameters, have been configured.
When commissioning is done, the LTMR controller is no longer locked, and is ready for operations. For information on operating states, see TeSys T LTMR Motor Management Controller User Guide.
First Power-up in the LTMCU
Using the LTMCU control operator unit, configuring the menu parameters clears the Controller System Config Required parameter and brings the LTMR controller out of initialization.
Click OK.
Click OK.
Click Yes to save the configuration.
When the configuration is saved, the First Setup menu is no longer displayed.
Send a Clear All command to the product to access the first setup menu again.
For more information, see the TeSys T LTMCU Control Operator Unit User’s Manual.
First Power-up in SoMove with theTeSys T DTM
Using SoMove with the TeSys T DTM to set all parameters, at the first power up of the LTMR controller, the Controller System Config Required parameter can be cleared by 2 ways:
-
In disconnected mode, by clicking to download the configuration files
-
In connected mode, by clicking after setting all parameters
Both commands bring the LTMR controller out of initialization.