FLC (Full Load Current) Settings
FLC Definition
The Full Load Current (FLC) represents the actual full-load current of the motor being protected by the LTMR controller. The FLC is a motor characteristic and can be found on the motor plate.
Many protection parameters are set as a multiple of FLC.
The FLC can be set from FLCmin to FLCmax.
Examples of FLC settings are detailed below.
Other Definitions
Load CT ratio = Load CT primary / (Load CT secondary * Passes)
Current sensor max = Current range max * Load CT ratio
Current range max is determined by the LTMR controller commercial reference. It is stored in units of 0.1 A and has one of the following values: 8.0, 27.0, or 100.0 A.
Contactor rating is stored in units of 0.1 A and is set by the user between 1.0 and 1000.0 A.
FLCmax is defined as the lower of the Current sensor max and the Contactor rating values.
FLCmin = Current sensor max / 20 (rounded to the nearest 0.01 A.). FLCmin is stored internally in units of 0.01 A.
-
The modification of the Contactor rating and/or Load CT ratio modifies the value of the FLC.
-
Do not set the FLC below the FLCmin.
Conversion of Amperes to FLC Settings
FLC values are stored as a percentage of FLCmax
FLC (in %) = FLC (in A) / FLCmax
Example 1 (No External CTs)
Data:
-
FLC (in A) = 0.43 A
-
Current range max = 8.0 A
-
Load CT primary = 1
-
Load CT secondary = 1
-
Passes = 1
-
Contactor rating = 810.0 A
Calculated parameters with one pass:
-
Load CT ratio = Load CT primary / (Load CT secondary * passes) = 1 / (1 * 1) = 1.0
-
Current sensor max = Current range max * Load CT ratio = 8.0 * 1.0 = 8.0 A
-
FLCmax = min (Current sensor max, Contactor rating) = min (8.0, 810.0) = 8.0 A
-
FLCmin = Current sensor max / 20 = 8.0 / 20 = 0.40 A
-
FLC (in %) = FLC (in A) / FLCmax = 0.43 / 8.0 = 5 %
Example 2 (No External CTs, Multiple Passes)
Data:
-
FLC (in A) = 0.43 A
-
Current range max = 8.0 A
-
Load CT primary = 1
-
Load CT secondary = 1
-
Passes = 5
-
Contactor rating = 810.0 A
Calculated parameters with five passes:
-
Load CT ratio = Load CT primary / (Load CT secondary * passes) = 1 / (1 * 5) = 0.2
-
Current sensor max = Current range max * Load CT ratio = 8.0 * 0.2 = 1.6 A
-
FLCmax = min (Current sensor max, Contactor rating) = min (1.6, 810.0) = 1.6 A
-
FLCmin = Current sensor max / 20 = 1.6 / 20 = 0.08 A
-
FLC (in %) = FLC (in A) / FLCmax = 0.43 / 1.6 = 27 %
Example 3 (External CTs, Reduced Contactor Rating)
Data:
-
FLC (in A) = 135 A
-
Current range max = 8.0 A
-
Load CT primary = 200
-
Load CT secondary = 1
-
Passes = 1
-
Contactor rating = 150.0 A
Calculated parameters with one pass:
-
Load CT ratio = Load CT primary / (Load CT secondary * passes) = 200 / (1 * 1) = 200.0
-
Current sensor max = Current range max * Load CT ratio = 8.0 * 200.0 = 1600.0 A
-
FLCmax = min (Current sensor max, Contactor rating) = min (1600.0, 150.0) = 150.0 A
-
FLCmin = Current sensor max / 20 = 1600.0 / 20 = 80.0 A
-
FLC (in %) = FLC (in A) / FLCmax = 135 / 150.0 = 90 %