Verify Configuration
Overview
The final step in the commissioning process is to verify that all configurable parameters used in the application are properly configured.
When performing this task, a main list of all the parameters to be configured and the desired settings is required. It is imperative to compare this list against the actual settings of the configured parameters.
Process
Verifying parameter settings is a three-part process:
-
Transfer the configuration file from the LTMR controller to the PC running SoMove with the TeSys T DTM. This allows to view the LTMR controller’s present parameter settings.
For information on transferring files from the LTMR controller to the PC, refer to the TeSys T DTM for SoMove FDT Container Online help.
-
Compare the main list of intended parameters and settings against the same settings located in the tab in SoMove with the TeSys T DTM. SoMove can be provided in the tab, the list of settings. It is a quick way to see what settings have been done.
-
Change the configuration settings as desired. Do this using:
-
Either SoMove with the TeSys T DTM, then download the edited file from the PC to the LTMR controller.
For information on transferring files from the PC to the LTMR controller, refer to the TeSys T DTM for SoMove FDT Container Online help.
-
Or LTMCU HMI: to edit parameters located in the Menu, navigate to the sub-menu settings and make the appropriate edits.
-