Wiring - Logic Outputs
Overview
The four logic outputs of the LTMR controller are relay outputs. The relay outputs command the motor managed by the LTMR controller.
The four relay outputs on the LTMR controller are:
-
Three single pole / single throw (SPST, NO) relay outputs
-
One double pole / single throw (DPST, NC+NO) relay output
Output Interposing Relays
When an output commands a contactor, an interposing relay may be required depending of the coil voltage and the power required by the contactor used.
The LTMR controller logic output characteristics are:
-
Rated insulation voltage: 300 V
-
AC rated thermal load: 250 Vac / 5 A
-
DC rated thermal load: 30 Vdc / 5 A
-
AC 15 rating: 480 VA, 500,000 operations, Ie max = 2 A
-
DC 13 rating: 30 W, 500,000 operations, Ie max = 1.25 A
If the LTMR controller logic output is not able to control directly the contactor, an interposing relay is required.
The protection module is mandatory on the interposing relays in order to suppress the surge.
Recommended Contactors
The tables in the appendix, listing the references and characteristics of Schneider Electric contactors, specify whether an interposing relay is required or not. Refer to the Recommended Contactors in the TeSys T LTMR Motor Management Controller User Guide.