Detecting Problems
Overview
The LTMR controller and the expansion module perform self-diagnostic checks at power-up and during operation.
Problems with either the LTMR controller or expansion module can be detected using
-
Power and Alarm LEDs on the LTMR controller,
-
Power and Input LEDs on the expansion module,
-
LCD Display on either a Magelis XBTN410 HMI device or a TeSys T LTMCU Control Operator Unit connected to the LTMR controller’s HMI port, or
-
SoMove with the TeSys T DTM running on a PC connected to the LTMR controller’s HMI port.
Device LEDs
The LEDs on the LTMR controller and expansion module can indicate the following problems:
|
LTMR LED |
LTME LED |
Problem |
||
|---|---|---|---|---|
|
Power |
Alarm |
PLC Alarm |
Power |
|
|
Off |
Solid red |
- |
- |
Internal trip |
|
On |
Solid red |
- |
- |
Protection trip |
|
On |
Flashing red (2x per second) |
- |
- |
Protection alarm |
|
On |
Flashing red (5x per second) |
- |
- |
Load shed or rapid cycle |
|
On |
- |
- |
Solid red |
Internal trip |
Magelis XBT HMI Device
The Magelis XBTN410 HMI automatically displays information about a trip or alarm, including LTMR controller self-diagnostic trips and alarms, when it occurs.
For information about the display of trips and alarms when the HMI is used in a one-to-many configuration, see Trips Management in TeSys T LTMR Motor Management Controller User Guide.
LTMCU Control Operator Unit
The TeSys T LTMCU Control Operator Unit automatically displays information about a trip or alarm.
For more information, see Trips and Alarms Display in TeSys T LTMCU Control Operator Unit User’s Manual.
SoMove with the TeSys T DTM
SoMove with the TeSys T DTM displays a visual array of active trips and alarms, including LTMR controller self-diagnostic trips and alarms, when these trips occur.
For information about this display of active trips and alarms, refer to the TeSys T DTM for SoMove FDT Container Online help.