DOCA0128EN-02

Assembly

Overview

This section describes how to assemble the LTMR controller and the LTME expansion module in a switchboard.

Connecting the LTMR Controller and the LTME Expansion Module

It is recommended to mount the LTMR controller and its LTME expansion module side by side with the LTME expansion module on the left side of the LTMR controller and connected by the LTMCC004 connecting jumper (1).

If it is not possible to mount the LTMR controller and its LTME expansion module side by side:

  • Use only the shielded cables LTM9CEXP03 (2) or LTM9CEXP10 (3) cables to connect them.

  • Ground the shielded cable.

  • Separate the LTM9CEXP•• connection cables from all other power or control cables to avoid EMC disturbance.

Example of Mounting in a Withdrawable Drawer of a Switchboard

A1, A2 LTMR controller power supply

B1, B2 Power supply dedicated to logic outputs

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?