DOCA0128EN-02

Configurable Parameters

Overview

The configurable parameters for the LTMR controller and the LTME expansion module are described below. The sequence of parameter configuration depends on the configuration tool utilized, either an HMI device or SoMove with the TeSys T DTM.

Parameters are grouped according to the TeSys T DTM parameter list tab. To help you find the link with the variable tables in the Use chapter, each parameter has its corresponding register number attached.

WARNING
RISK OF UNINTENDED CONFIGURATION AND OPERATION
When modifying parameter settings of the LTMR controller:
  • Be especially careful if you change parameter settings when the motor is running.
  • Disable network control of the LTMR controller to prevent unintended parameter configuration and operation.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?