Wiring - Temperature Sensors
Temperature Sensors
The LTMR controller has two terminals dedicated to motor temperature sensing protection: T1 and T2. These terminals return the temperature value measured by resistance temperature detectors (RTDs).
One of the following types of motor temperature sensor can be used:
-
PTC Binary
-
PT100
-
PTC Analog
-
NTC Analog
For more information on temperature sensors, refer to the TeSys T LTMR Motor Management Controller User Guide.
Temperature Sensor Wiring
The following table shows the maximum wire lengths for temperature sensor elements:
|
Wire Size |
0.5 mm2 (AWG 20) |
0.75 mm2 (AWG 18) |
1.5 mm2 (AWG 16) |
2.5 mm2 (AWG 14) |
|
Maximum Wire Length |
220 m (656 ft) |
300 m (985 ft) |
400 m (1312 ft) |
600 m (1970 ft) |
Use unshielded twisted pair cable to connect the controller to the temperature sensor.
For the controller to accurately measure the resistance of the temperature-sensing element, you must measure the resistance of the twisted-pair and add it to the desired resistance for protection. This compensates for the lead resistance.
For more information about wiring, see Wiring Generalities.