DOCA0128EN-02

Dimensions

Overview

This section presents the dimensions of the LTMR controller and the LTME expansion module, as well as the dimensions of the clearance zone around the controller and the expansion module. Dimensions are given in both millimeters and inches and apply to all LTMR and LTME models.

LTMR Controller Dimensions

NOTE: The height of the controller may increase when using alternate wiring terminals.

LTME Expansion Module Dimensions

Clearance Zone Dimensions

For EMC (Electromagnetic Compatibility), it is recommended to mount a contactor at a distance of more than 5 cm (1.97 in) from the LTMR controller and LTME expansion module.

The maximum rated ambient temperature of the controller depends on the clearance zone dimensions. They are shown in the following table.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?