DOCA0197EN-01

Connected Devices

It is recommended to regularly check the list of devices connected to the IEEE 802.15.4 network of the Panel Server . In the case of an unknown connected device, locate it and remove it. You can also rebuild the network and reconnect only identified devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.