DOCA0197EN-01

Bluetooth® Low Energy Communication

Presentation

Using Bluetooth® Low Energy functionality, you can access the Wireless Panel Server from a smartphone running EcoStruxure Power Commission App.

You can establish a Bluetooth Low Energy connection with only one Wireless Panel Server at a time. Only one smartphone at a time can connect to a Wireless Panel Server .

Prerequisites for Using Bluetooth Low Energy

The prerequisites for establishing a Bluetooth Low Energy connection are:

  • The Wireless Panel Server must be powered.

  • Bluetooth Low Energy communication must be activated on the Wireless Panel Server . See Activating/Deactivating Bluetooth Low Energy Communication .

  • You must have a smartphone running EcoStruxure Power Commission App.

  • The smartphone must support Android 8.0 or iOS 13 or above, and be compatible with Bluetooth Low Energy (a Bluetooth feature supported since Bluetooth version 4.0).

  • You must have access to the Wireless Panel Server , and be physically within an open field range of up to 10 meters in front of the switchboard for optimized connection for the duration of the connection.

Activating/Deactivating Bluetooth Low Energy Communication

By default, Bluetooth Low Energy communication is deactivated.

To activate Bluetooth communication on the Wireless Panel Server :

  1. Check that the Wireless Panel Server is in normal operation (status LED steady green).

  2. Briefly press the Wireless Panel Server pushbutton (less than 5 s).

    Result:

    • The status LED blinks blue when Bluetooth communication is activated and Wireless Panel Server is ready to connect to EcoStruxure Power Commission App.

    • The LED turns steady blue when the Wireless Panel Server is connected to EcoStruxure Power Commission App.

  3. To deactivate Bluetooth Low Energy communication, press the pushbutton again.

Establishing a Bluetooth Low Energy Connection

Proceed as follow to establish a Bluetooth Low Energy connection from your smartphone to the Wireless Panel Server :

  1. Start EcoStruxure Power Commission App on your smartphone.

  2. Select the Wireless Panel Server to which you want to connect.

  3. Scan the QR code on the front face of the Wireless Panel Server .

  4. On the Wireless Panel Server , briefly press the pushbutton (less than 5 s).

    Result: The status LED lights up and starts blinking blue.

  5. When the connection is established, the status LED turns steady blue.

  6. To end the connection, you can disconnect from EcoStruxure Power Commission App.

Troubleshooting Bluetooth Low Energy Communication Issues

The following table lists common problems when establishing a Bluetooth connection to the Wireless Panel Server .

Problem description Probable causes Solutions
The Bluetooth connection was established but the signal is lost. The smartphone has been moved out of range. Place the smartphone within the range for Bluetooth and establish a new connection.
The status LED is steady blue on the Wireless Panel Server but your smartphone is not connected to the Wireless Panel Server . A smartphone is already connected to the Wireless Panel Server . Check whether another smartphone within range is also connected to the Wireless Panel Server .

Security Feature

Bluetooth Low Energy communications are encrypted using Advanced Encryption Standard (AES) 128-bit encryption. The LE Secure Connections pairing model helps ensure protection against passive eavesdropping.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.