DOCA0197EN-01

Security Recommendations for Maintenance

Over the lifetime of the Wireless Panel Server , it is recommended to regularly perform the following operations:

  • Check physical security of the Wireless Panel Server (see Hardware Description for location of the tamper-indicating labels).

  • Make sure that you have the latest firmware update. You should have registered to receive security notifications.

  • Check the connected devices for the presence of unknown devices.

  • Check the audit logs for unexpected behaviors such as invalid login attempts or frequent rebooting.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.