DOCA0197EN-01

Security Recommendations for Operation

Firmware Update

It is recommended to keep the Wireless Panel Server firmware up to date (see detailed topic). Firmware update is managed with EcoStruxure Power Commission App.

Secure Communication with Wireless Devices

It is recommended to periodically verify the list of paired devices configured in the Wireless Panel Server by using EcoStruxure Power Commission App and make sure that the list of devices is up to date and contains no unexpected or rogue devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.