DOCA0197EN-01

Hardware Description

Description

Wireless Panel Server embedded in a PrismaSeT P Active switchboard

  1. LoRa antenna

  2. Voltage presence indicator LEDs

  3. QR code to product information and cloud service activation

  4. Pushbutton:

    • Activate/Deactivate connection to Bluetooth wireless technology

    • Reboot Wireless Panel Server

    • Reset Wireless Panel Server to factory settings

  5. Wireless Panel Server status LED

  6. Power supply and voltage inputs connector

  7. Tamper-indicating label affixed folded on rear and bottom sides

  8. Gasket

  9. SMA connector for LoRa antenna

  10. Wiring harness


For information on installation, consult the instruction sheet available on the Schneider Electric website: NNZ50846 .

@Translator: see NNZ50846-0x

Wireless Panel Server - Rear view

 

Wireless Panel Server - Front view

 

Wireless Panel Server - Bottom view

   

Wiring harness

LoRa antenna

Voltage Presence Indicator LEDs

The LEDs L1, L2, and L3 indicate the phase status (presence or absence of voltage).
LED indication Description
LED ON (white) Voltage detected
LED OFF Absence of voltage
3 LEDs blinking Firmware update in progress

Wireless Panel Server Status LED

The status LED indicates the operation mode and Bluetooth communication status of the Wireless Panel Server .
LED indication Description
Wireless Panel Server power supply not connected or inoperative.
Power supply connected and connection to LoRa network is established.
Attempt to connect to LoRa network.
Wireless Panel Server is booting.

During commissioning, Wireless Panel Server power supply is connected but LoRa communication has not been activated for more than 15 minutes.

NOTE: During operation, malfunction is detected. Connect Wireless Panel Server to EcoStruxure Power Commission App to diagnose the issue.

Major malfunction detected. Wireless Panel Server communication with EcoStruxure Power Commission App not possible for diagnosis. The Wireless Panel Server must be replaced.
Firmware discrepancy or major malfunction detected. Connect Wireless Panel Server to EcoStruxure Power Commission App to diagnose the issue. Depending on issue, the Wireless Panel Server may need to be replaced.
Bluetooth wireless technology activated and Wireless Panel Server connected to EcoStruxure Power Commission App.
Bluetooth wireless technology activated and Wireless Panel Server ready to connect to EcoStruxure Power Commission App.

Pushbutton

Rebooting Wireless Panel Server

To reboot the Wireless Panel Server :

  1. Press and hold the pushbutton for more than 5 seconds.

  2. Release the pushbutton.

  3. The status LED turns steady orange while the Wireless Panel Server is rebooting.

  4. The status LED turns blinking green while the Wireless Panel Server is attempting to connect to LoRa network.

  5. Finally, the status LED turns steady green indicating that the Wireless Panel Server is connected to a LoRa network.

NOTE: The status LED blinks orange if connection to a LoRa network is not possible.

Resetting Wireless Panel Server to Factory Settings

To reset the Wireless Panel Server to factory settings:

  1. Power off the Wireless Panel Server (Unplug the power supply connector).

  2. Power on the Wireless Panel Server (Plug the power supply connector).

  3. Press and hold the pushbutton until the status LED is fast blinking orange.

    NOTE: A continuously pressed pushbutton from the boot results to a factory reset.
  4. Within 5 seconds of seeing the status LED fast blinking orange, release the pushbutton and press it back again.

  5. If the pushbutton is pressed as mentioned in step 4:

    • The status LED is fast blinking green.

    • Then, the status LED turns steady orange while the Wireless Panel Server is rebooting.

    • Then, the status LED turns blinking green while the Wireless Panel Server is attempting to connect to LoRa.

    • Finally, the status LED turns steady green indicating that the Wireless Panel Server is connected to a LoRa network.

    NOTE: The status LED blinks orange if connection to a LoRa network is not possible.
  6. If the pushbutton is not pressed as mentioned in step 4:

    • If the status LED turns steady red, the factory reset is cancelled.

    • If the status LED starts blinking red, reboot the Wireless Panel Server . It is not reset to factory settings.

QR Code

You can scan the QR code on the front face of a PrismaSeT Active switchboard with a smartphone running a QR code reader and connected to the Internet. It redirects to download EcoStruxure Facility Expert App or open it if you already have it installed on your mobile device.

If... Then...
the Wireless Panel Server is not yet connected to Schneider Electric cloud it opens the activation wizard to connect the Wireless Panel Server .
the Wireless Panel Server is connected to Schneider Electric cloud you can access your connected PrismaSeT Active switchboard or request access to it.

When accessing the Go2SE landing page, the following information is displayed:

  • Wireless Panel Server commercial reference and serial number

  • Wireless Panel Server technical characteristics

  • Wireless Panel Server technical publications

Tamper Detection

A tamper-indicating label helps detect unauthorized physical access into the Wireless Panel Server . One tamper-indicating label is affixed folded on rear and bottom of the Wireless Panel Server .

External LoRa Antenna

An external LoRa antenna (SMT10015) must be connected to the Wireless Panel Server and installed outside the switchboard. The antenna is required for LoRaWAN communication.

For information about antenna installation including antenna location:

  • See DOCA0203EN PrismaSeT Active  - Installation and Maintenance Guide .

  • Access the demonstration video by clicking here.

High Service Level

To help ensure a high communication service level, Schneider Electric recommends that the Wireless Panel Server is replaced every 10 years.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.