DOCA0197EN-01

Configuration of PrismaSeT Active Switchboards with Wireless Devices

Objectives

Configure the wireless devices installed in the PrismaSeT Active switchboard.

Pre-requisites

  • A smartphone running a QR code reader and compatible with Bluetooth Low Energy wireless technology.

  • EcoStruxure Power Commission App installed on smartphone. For information about downloading the App, see the detailed topic.

  • The switchboard that embeds the Wireless Panel Server must be energized and the Wireless Panel Server status LED blinking orange.

Configuring the Switchboard with Wireless Devices

To configure the switchboard with wireless devices through EcoStruxure Power Commission App, proceed as follows:

  1. Scan the QR code on the front face of the Wireless Panel Server using the smartphone camera.

  2. In the Go2SE landing page that opens, click the EcoStruxure Power Commission App section.

  3. Follow the instructions to register to EcoStruxure Power Commission .

  4. Activate Bluetooth communication on your smartphone.

  5. Briefly press the button (less than 5 s) on the Wireless Panel Server to activate Bluetooth communication.

    Result: The status LED blinks blue when the connection procedure is in progress, then turns steady blue when the Bluetooth connection is established from the Wireless Panel Server to the smartphone.

  6. Set the Wireless Panel Server password (at first connection).

  7. If necessary, update firmware.

  8. Follow the instructions to discover the wireless devices installed in the switchboard.

  9. Associate the discovered wireless devices to the Wireless Panel Server .

  10. Configure each wireless device associated to the Wireless Panel Server .

  11. Generate the setup report for Factory Acceptance Tests (FAT).

  12. Activate cloud service with EcoStruxure Facility Expert App (see procedure).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.