DOCA0197EN-01

Introduction

SeT Series Master Range

Featuring outstanding medium-voltage (MV) and low-voltage (LV) switchboards, motor control centers and power distribution solutions for high-performance power applications, Schneider Electric's SeT Series is best-in-class solutions based on high levels of safety and an optimized footprint. Built on a modular architecture and incorporating smart connected devices for maximum safety, reliability, performance and energy efficiency, the SeT Series is delivered to customers directly from our Schneider Electric plants or via a global network of licensed partner panel builders, who are trained and audited to provide quality equipment and support.

Overview

The Wireless Panel Server is a gateway embedded in the roof of PrismaSeT P Active or PrismaSeT G Active switchboards, enabling wireless connectivity to Schneider Electric cloud.

The Wireless Panel Server offers the following advantages and services:

  • Switchboard voltage loss monitoring

  • Fire prevention in electrical distribution switchboards

  • Power availability alarming

  • Energy consumption management

The Wireless Panel Server provides monitoring of the switchboard via EcoStruxure Facility Expert software.

Features

The Wireless Panel Server provides the following features:

The features depend on the PrismaSeT Active switchboard in which the Wireless Panel Server is embedded.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.