DOCA0197EN-01

Device Characteristics

Overview

The Wireless Panel Server is equipped with security-enabling features. These features come in a preset state and can be modified to meet your installation needs. This guide provides recommendations to help secure your Wireless Panel Server .

Wireless Panel Server Interfaces

The Wireless Panel Server communicates through the following wireless communication interfaces:

  • LoRaWAN for communication with the cloud.

  • Bluetooth Low Energy for communication with a mobile device such as a smartphone or tablet.

  • Wireless protocol for communication with wireless devices, using radio frequency communication ISM band 2.4 GHz.

The Wireless Panel Server does not implement IP-based protocols on any of the three interfaces.

NOTE: The Wireless Panel Server does not support any Ethernet-based physical interface and cannot be connected to an Ethernet Local Area Network (LAN).

Supported Protocol

The Wireless Panel Server supports the Constrained Application Protocol (CoAP) over Bluetooth wireless technology for configuration through EcoStruxure Power Commission App.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.