Voltage Loss Function
Presentation
WARNING |
|---|
|
HAZARD OF NON-DETECTION OF VOLTAGE
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The voltage loss alert function provides local and remote visibility if an electrical outage or abnormal voltage phase conditions have occurred. It makes voltage status inspection faster and diagnosis more efficient, helping to prevent equipment damage, and helping the operation team to respond without delay.
Remote Voltage Loss Alert
When voltage loss is detected by a Wireless Panel Server communicating through LoRa and that service for EcoStruxure Facility Expert App is activated, a notification is sent on mobile devices (smartphone or tablet) for the following alerts:
- Phase loss alert.
- Power outage alert of the switchboard if the voltage presence indicator is cabled from downstream the main incomer.
- Power outage alert upstream of the switchboard if the voltage presence indicator is cabled upstream from the main incomer (with an additional protection).
-
If one phase loss occurs, the voltage presence indicator LED is on with no alert sent. It is due to a probability of residual voltage coming back on the phase from the loads.
-
If two or three phase loss occurs, the voltage presence indicator LEDs switch off and a voltage loss alert is triggered.
Voltage Presence Indicator in Single-Phase Network
In a single-phase network, the voltage presence indicator LED operates as follows:
| If... | Then... |
|---|---|
| Phase is disconnected | The voltage presence indicator LED is off and the Wireless Panel Server communication through LoRa is operational. |
| Neutral is disconnected | The voltage presence indicator LED is off and the Wireless Panel Server communication through LoRa is not operational. |
Setting the Parameters
Alerts provided by the voltage loss function are set with EcoStruxure Facility Expert App and require LoRa communication.
WARNING