DOCA0197EN-01

EcoStruxure Power Commission App

Overview

EcoStruxure Power Commission App helps you to manage commissioning, testing, and maintenance of the Wireless Panel Server . The embedded, innovative features provide simple ways to configure, test, and commission the smart electrical devices.

EcoStruxure Power Commission App automatically discovers smart devices and allows you to add the devices for an easy configuration. You can generate a comprehensive report to have a complete view of all devices installed in the Wireless Panel Server .

The EcoStruxure Power Commission App enables the configuration of the Wireless Panel Server .

Key Features

EcoStruxure Power Commission App performs the following actions for the supported devices :

  • Configure the Wireless Panel Server

  • Add wireless devices to the Wireless Panel Server

  • Configure the wireless devices:

    • Device identification

    • Electrical information

    • Contextualization data

  • Generate Wireless Panel Server report

  • Download Wireless Panel Server logs (audit and event logs)

Downloading the Application

To download the EcoStruxure Power Commission App:

  • Scan the QR code on the front face of the Wireless Panel Server to access the Go2SE landing page and the EcoStruxure Power Commission App section.

  • Or scan the following QR code:

For More Information

For more information about commissioning PrismaSeT Active switchboards through EcoStruxure Power Commission App:

  • See ESXP1G005EN EcoStruxure™ Power - Commissioning Guide for Digital Solutions based on PrismaSeT Active .

  • Access the demonstration video by clicking here

    .

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.