DOCA0197EN-01

Commissioning

Overview

Commissioning the Wireless Panel Server depends on whether wireless devices are installed in the PrismaSeT Active switchboard that embeds the Wireless Panel Server .

Wireless Panel Server switchboard type Commissioning procedure
Without wireless devices

Activate cloud service with EcoStruxure Facility Expert App.

With wireless devices
  1. Configure the switchboard and wireless devices with EcoStruxure Power Commission App.

  2. Activate cloud service with EcoStruxure Facility Expert App.

For more information about commissioning your connected PrismaSeT Active switchboard, see ESXP1G005EN EcoStruxure™ Power - Commissioning Guide for Digital Solutions based on PrismaSeT Active .

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.