DOCA0197EN-01

EcoStruxure Facility Expert App

Overview

Based on latest technology merging, mobile App, web platform and IoT, EcoStruxure Facility Expert helps you to optimize field operations, reduce energy consumption and help ensure business continuity. EcoStruxure Facility Expert is also used to establish connection of a PrismaSeT Active switchboard with an embedded Wireless Panel Server to the Schneider Electric cloud.

EcoStruxure Facility Expert provides the following features for free:

  • QR code creation

  • Asset status and map localization

  • Asset log history and reference document library

  • Maintenance plan and task reminders

  • Task manager features (for example, task assignment, notifications)

  • One-click intervention reports

  • Collaborative features (for example, chat, information sharing)

  • Voltage loss alert function with notifications on mobile devices (tablet or smartphone)

  • Load energy index on mobile devices

To enable advanced functionalities and access more values, subscribe to:

  • EcoStruxure Facility Expert - Operations to monitor the Wireless Panel Server and loads condition

  • EcoStruxure Facility Expert - Energy to monitor energy consumption per site, zone, and usage

EcoStruxure Facility Expert - Operations Subscription

Providing relevant information on key assets and sending remote alarms EcoStruxure Facility Expert - Operations allows to diagnose remotely in case of issue and to manage maintenance more efficiently.

In addition to the free EcoStruxure Facility Expert features, Operations subscription provides the following:

  • Alerts on power outage with causes identification and recommendations

  • Notification on mobile devices

  • Task manager and collaboration features

  • Data storage, asset history and reports

  • Load energy metering

EcoStruxure Facility Expert - Energy Subscription

EcoStruxure Facility Expert - Energy allows continuous monitoring and trends.

EcoStruxure Facility Expert - Energy provides the following features:

  • Energy consumption per site, per usage and per zone

  • Alerts for over-target energy consumption

  • Cost allocation

  • Power demand monitoring

  • Aggregated or multi-site comparison view

  • Monthly scorecards

Downloading the Application

To download the EcoStruxure Facility Expert App:

  • Scan the QR code on the front face of the Wireless Panel Server to access the Go2SE landing page and the EcoStruxure Facility Expert App section

  • or scan the following QR code:

For More Information

  • For more information about how to handle EcoStruxure Facility Expert App from account creation to connected features, see ESXUG001EN EcoStruxure Facility Expert Starter Guide for Operations . This guide contains detailed information about:

    • EcoStruxure Facility Expert App subscriptions

    • Creating and managing EcoStruxure Facility Expert account

    • Creating asset library:

      • Register assets manually

      • Create maintenance tasks

      • Download assets from Schneider Electric resource repository by scanning product QR code

    • Operating with EcoStruxure Facility Expert App and manage your asset library:

      • Share information and collaborate

      • Operate assets and manage tasks

      • Access history and asset trending

      • Receive alerts from the equipment

  • For quick start with EcoStruxure Facility Expert , see demonstration videos: https://www.productinfo.schneider-electric.com/ecofacilityexpert/

  • For more information about how to establish the connection of the Wireless Panel Server to Schneider Electric cloud and about commissioning your connected PrismaSeT Active switchboard, see ESXP1G005EN EcoStruxure™ Power - Commissioning Guide for Digital Solutions based on PrismaSeT Active .

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.