DOCA0197EN-01

User Access Control

Presentation

User access to the Wireless Panel Server through the local Bluetooth Low Energy interface is done by using EcoStruxure Power Commission App and is password-protected. Once the user is successfully logged into the Wireless Panel Server , the user has access to all capabilities and functions of the Wireless Panel Server .

User Login

EcoStruxure Power Commission App is the tool for logging in to and commissioning the Wireless Panel Server . Before login, the smartphone must be paired with the Wireless Panel Server (see detailed topic).

Changing Password

At first connection to the EcoStruxure Power Commission App, the user is prompted to set the password.

To change the password, proceed as follows:

  1. Activate Bluetooth wireless technology on the Wireless Panel Server .

  2. Pair your smartphone to the Wireless Panel Server .

  3. Use EcoStruxure Power Commission App to log in to the Wireless Panel Server .

  4. Change the password.

Password Requirements

A password must conform to the following rules:

  • 6 to 32 characters

  • At least one character in uppercase

  • At least one character in lowercase

Password Lockout

In case of 10 invalid attempts to log in to the Wireless Panel Server , user access is locked. It remains locked for 10 minutes before the user can attempt to log in again.

Consecutive invalid attempts (up to 14) lock user access for 10 minutes after each invalid attempt.

After the fifteenth consecutive invalid attempts, the user access is locked for 60 minutes after each invalid attempt.

User account lock state remains if the Wireless Panel Server is rebooted, including reboot after power loss.

To unlock user access, the user must log in successfully after a lock period or apply the forgotten password process using EcoStruxure Power Commission App.

Password Forgotten

If the user has forgotten the Wireless Panel Server password, the following requirements must be followed:

  • The user must connect the smartphone to the Wireless Panel Server and open the EcoStruxure Power Commission App.

  • The user must have physical access to the Wireless Panel Server to press the Wireless Panel Server pushbutton.

Following the forgotten password process will result in losing the Wireless Panel Server configuration:

  • The user password is reset.

  • Configured devices are decommissioned (IEEE 802.15.4 wireless devices are unpaired and removed from configuration).

  • The Wireless Panel Server reboots.

  • The user is prompted to set a new password after Wireless Panel Server reboot.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.