Voltage Presence Indicators
Presentation
WARNING |
|---|
|
HAZARD OF NON-DETECTION OF VOLTAGE
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
L1, L2, and L3 LEDs on the Wireless Panel Server front face provide voltage presence indication. For information about the location and description of the voltage presence indicator LEDs, see hardware presentation.
Wiring Harness Connection
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Always connect the Wireless Panel
Server
terminal block to incoming cables or busbars by using the wiring
harness SMT10016 provided with the Wireless Panel
Server
. If using own cables, make sure appropriate short-circuit protection
is added.
Failure to follow these instructions will result in death or serious injury.
|
Voltage Presence Indicators
For each phase, the voltage presence indicator LED is on if voltage is present on phase.
-
If one phase loss occurs, the voltage presence indicator LED is on with no alert sent. It is due to a probability of residual voltage coming back on the phase from the loads.
-
If two or three phase loss occurs, the voltage presence indicator LEDs switch off and a voltage loss alert is triggered.
| If... | Then... |
|---|---|
| Phase is disconnected | The voltage presence indicator LED is off and the Wireless Panel Server communication through LoRa is operational. |
| Neutral is disconnected | The voltage presence indicator LED is off and the Wireless Panel Server communication through LoRa is not operational. |
Troubleshooting Voltage Presence Indicator LED Issues
|
Problem |
Diagnostics |
Action |
|---|---|---|
| None of the voltage presence indicator LEDs are lit. | Source power is not applied or is not stable. | Apply power or check power source. |
| Only one voltage presence indicator LED is lit. | Check your installation: single phase or 3-phase. |
|
| During commissioning, before connection to EcoStruxure Facility Expert App, one of the voltage presence indicator LEDs is not lit. | The phase is lost. | Check cable connection on phase. |
| The phase is not correctly connected. |
WARNING
DANGER