DOCA0197EN-01

Cloud Service Activation

Objectives

  • Activate the Wireless Panel Server cloud connection (LoRa network).

  • Activate the voltage loss function on EcoStruxure Facility Expert App.

Pre-requisites

  • Be on site and have access to the QR code on the front face of the Wireless Panel Server from a smartphone.

  • A smartphone running a QR code reader.

  • EcoStruxure Facility Expert App installed on smartphone. For information about EcoStruxure Facility Expert App, see the detailed topic.

  • The switchboard that embeds the Wireless Panel Server must be energized and the Wireless Panel Server status LED blinking orange.

Activating the Cloud Service

To activate the cloud service through EcoStruxure Facility Expert App, proceed as follows:

  1. Scan the QR code on the front face of the Wireless Panel Server using the smartphone camera.

  2. In the Go2SE landing page that opens, click the EcoStruxure Facility Expert App section.

  3. Follow the instructions to register to EcoStruxure Facility Expert .

  4. The PrismaSeT connection wizard opens automatically. Follow the instructions on screen.

  5. Wait for the Wireless Panel Server to connect to LoRa network. It can take several minutes (status LED blinking green).

    • When the LoRa connection is established:

      • The status LED turns steady green.

      • The EcoStruxure Facility Expert App displays a message of successful connection to LoRa network.

    • If the LoRa connection is not successful, see ESXP1G005EN EcoStruxure™ Power - Commissioning Guide for Digital Solutions based on PrismaSeT Active .

  6. Activate cloud service through EcoStruxure Facility Expert App. For detailed information, see ESXP1G005EN EcoStruxure™ Power - Commissioning Guide for Digital Solutions based on PrismaSeT Active

    NOTE: In case of no internet connection, move to a place with internet connection to finish the activation. As soon as the smartphone detects an internet network, it automatically updates the information.

  7. You can monitor the status of the switchboard with EcoStruxure Facility Expert App.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.