DOCA0197EN-01

Security Recommendations for Decommissioning

The Wireless Panel Server is configured with confidential information, such as user account identifiers. When disposing of the Wireless Panel Server, it is required to reset it to make sure that no sensitive or confidential information can be disclosed or reused.

NOTICE
LOSS OF GATEWAY FUNCTION
  • Only decommission Wireless Panel Server when it is no longer needed.
  • If you decommission Wireless Panel Server, you will not be able to receive voltage loss alarm for PrismaSeT Active Switchboard Resetting gateway removes all the configuration and configured devices are decommissioned.
Failure to follow these instructions can result in non-operational system where the Wireless Panel Server is installed.

Reset Procedure

To reset the Wireless Panel Server , follow the below procedure to set the configuration settings to factory values:

  1. Launch EcoStruxure Power Commission App and scan the Wireless Panel Server QR code.

  2. Connect to the Wireless Panel Server .

  3. Unpair all wireless devices from the Wireless Panel Server .

  4. Finalize the commissioning.

  5. Disconnect from the Wireless Panel Server .

  6. Re-Launch EcoStruxure Power Commission App.

  7. Scan the Wireless Panel Server QR code.

  8. Click on Forgotten password.

  9. Follow the instruction on the EcoStruxure Power Commission App:

    • The Wireless Panel Server LED will blink orange fast.

    • You will have 5 seconds to press the pushbutton next to the LED to validate the reset operation.

    • Result: The status LED blinks fast green indicating that reset to factory setting is confirmed.

  10. Wait for the Wireless Panel Server to restart completely:

    • The status LED turns steady orange while the Wireless Panel Server is booting. After the booting the status LED will blink green for fifteen minutes.

    • The status LED turns steady green when the Wireless Panel Server is in normal operation.

      IMPORTANT: After performing a reset to factory setting on the Wireless Panel Server that has been previously connected to the Schneider Electric cloud, contact the Schneider Electric Customer Care Center to finalize the decommissioning.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.