DOCA0197EN-01

Wireless Panel Server System

Architecture

The following illustration shows a possible architecture of the Wireless Panel Server .

LoRa communication
Bluetooth® communication
IEEE 802.15.4 wireless communication
  1. EcoStruxure Power Commission App for wireless devices configuration

  2. EcoStruxure Facility Expert cloud-based software:

    • Voltage loss notification

    • Alert system (Operations subscription)

    • Energy management through webpages (Energy subscription)

Supported Wireless Devices

The following table presents the IEEE 802.15.4 wireless devices in a PrismaSeT switchboard which can communicate with the embedded Wireless Panel Server .

Application Wireless device Description

Fire prevention

HeatTag sensors

Innovative smart sensor, able to analyze gas and particles in the switchboard and alert before any smoke or insulator browning occurs.

Acti9 Active

Arc Fault Detection Device that helps protect circuits against short-circuits and overcurrent, persons against earth-leakage, and assets thanks to inbuilt arc flash detection device.

Power availability

Wireless indication auxiliary for ComPacT NSX and ComPacT NSXm

Wireless indication auxiliary that provides remote and local information about the circuit breaker status (open, close, trip, trip on electrical default).

Energy management

PowerTag Energy sensors

Compact and easy-to-install Class 1 wireless communication energy sensor that monitors and measures energy and power in real-time. PowerTag Energy sensor sends alerts in the event of an electrical anomaly.

Maximum Configuration

The maximum number of supported wireless devices which can be connected to a Wireless Panel Server is as follows:

  • Up to 3 HeatTag sensors

  • Up to 15 PowerTag Energy sensors if no HeatTag sensors connected

  • Up to 10 PowerTag Energy sensors if one or several HeatTag sensors are connected

Commercial References

The following table indicates the commercial references and designation of Wireless Panel Server parts and spare parts:

Commercial reference Designation
SMT10011 Cable extender for LoRa antenna (5 m)
SMT10013 LoRa tester
SMT10014 LoRa/4G gateway
SMT10015 Spare LoRa antenna for Wireless Panel Server
SMT10016 Spare wiring harness for Wireless Panel Server
SMT10019 Spare Wireless Panel Server

For more information, see DESW026EN PrismaSeT  P Active  - Catalogue or DESW027EN PrismaSeT  G Active  - Catalogue .

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.